R_TMRX_Set_PowerOff


Halts the clock supplied to the 16-bit timer RX.

Remark

Calling this API function changes the 16-bit timer RX to reset status.
For this reason, writes to the control registers after this API function is called are ignored.

[Syntax]

void    R_TMRX_Set_PowerOff ( void );

[Argument(s)]

None.

[Return value]

None.