R_TMRX_Get_BufferValue


Reads the buffer value of TRX register (16-bit timer RX).

[Syntax]

#include    "r_cg_macrodriver.h"
void   R_TMRX_Get_BufferValue ( uint32_t * const value );

[Argument(s)]

I/O

Argument

Description

O

uint32_t
  * const value;

Pointer to an area storing the buffer resister value of TRX resister

[Return value]

なし