r_uartfn_callback_error


Performs processing in response to the LIN-UART reception status interrupt INTLS.

Remark

This API function is called as the callback routine of interrupt process r_uartfn_interrupt_error corresponding to the LIN-UART reception status interrupt INTLS.

[Syntax]

static  void    r_uartfn_callback_error ( uint8_t err_type );

Remark

n is the channel number.

[Argument(s)]

I/O

Argument

Description

O

uint8_t err_type;

Trigger for LIN-UART reception status interrupt

00000xx1B: Overrun error

00000x1xB: Parity error

000001xxB: Framing error

[Return value]

None.