r_uartfn_callback_idmatch


Performs processing in response to match ID parity.

Remark

This API function is called as the callback routine of interrupt process r_uartfn_interrupt_error corresponding to the LIN-UART reception status interrupt INTLS (performed when ID parity has been matched).

[Syntax]

static  void    r_uartfn_callback_idmatch ( void );

Remark

n is the channel number.

[Argument(s)]

None.

[Return value]

None.