Port Setting dialog box


This dialog box sets a COM port on the host machine to which communication from the microcontroller is redirected.

Figure A.66

Port Setting Dialog Box

 

This section describes the following.

[How to open]

-

On the Debug Console panel, select [COM Port...] from the context menu.

[Description of each area]

(1)

[COM Port] area

Select a COM port to which communication is redirected. If there are no COM ports available on the host machine, this drop-down list is blank.

(2)

[Baudrate] area

Select a baud rate at which communication is performed with the redirected COM port.

The drop-down list displays the following baud rates. If "System" is selected, the baud rate set by the device manager applies.

System, 1200, 2400, 4800, 9600, 19200, 38400, 115200

[Function buttons]

Button

Function

Connect/Disconnect

Connects to (default) or disconnects from a COM port.

When connected to a COM port, the button is labeled "Disconnect."

When disconnected from a COM port, the button is labeled "Connect."

Cancel

Nullifies COM port settings and closes this dialog box.

Help

Displays help for this dialog box.