Combination Condition dialog box [E1] [E20] [EZ Emulator]


This dialog box is used to change the detailed information on combination condition for the combination break or for the trace event selected on the Events panel.

Remark

See "2.17.7 Points to note regarding event setting" for details on event setting.

Figure A.59

Combination Condition Dialog Box (Combination Break)

Figure A.60

Combination Condition Dialog Box (Trace Event)

 

This section describes the following.

[How to open]

-

On the Events panel, move the caret to the combination break of which you wish to change the detailed information, then select [Edit Condition...] from the context menu.

-

On the Events panel, move the caret to the trace of which you wish to change the detailed information, then select [Edit Condition...] from the context menu.

[Description of each area]

(1)

Tab selection area

You can display the detailed information on combination conditions by the selection of a tab. Types of tabs to be displayed will differ depending on the event you have selected on the Events panel.

Combination break

Only [Break] tab is displayed.

Trace

[Start Condition] tab and [End Condition] tab are displayed. By switching, you can set the combination condition for each tab.

(2)

Combination condition selection area

(a)

[Combination]

Select the conditions from the following drop-down list.

Conditions

Functions

OR

The condition is satisfied when one of the set events is encountered.

AND

The condition is satisfied when all the set events are encountered irrespective of the time line.

Sequential

The condition is satisfied when the set events are encountered in the specified sequence.

Caution

Also see Cautions of "(1) Editing the combination condition" for details on combination conditions.

(3)

Object event condition display area

(a)

Display of the list

The object events to be combined are shown in the list.

No.

The events in the list are numbered from top to bottom. This item is displayed only when you have specified [Sequential] for the combination conditions. For the condition to be satisfied, events must be encountered in the order indicated by these numbers.

Event

Detailed information on event conditions is displayed.

It is identical to the information displayed on the Events panel.

(b)

Buttons

Buttons

Functions

Up

Moves the event serial number upward in the Object event list. This button is enabled only when you have specified [Sequential] for the combination conditions.

Down

Moves the event serial number downward in the Object event list. This button is enabled only when you have specified [Sequential] for the combination conditions.

R Event

Moves the event selected in the Object event list to the Reset event list. This button is enabled only when you have specified [Sequential] for the combination conditions.

(4)

Reset event condition display/cancel area

(a)

Display of the list

Detailed conditions are displayed for the event which has been registered as a reset event. When the reset event displayed in this list is encountered, all the other event conditions which have been holding until then will be cleared.

Caution

Also see Cautions of "(3) Editing the reset event" for details on Editing the reset event.

(b)

Button

Button

Function

Cancel

Moves the event inside the Reset event list to the Object event list. This button is enabled only when you have specified [Sequential] for the combination conditions.

[Function buttons]

Buttons

Functions

OK

Applies the detailed settings specified in the dialog box to the combination break or to the trace and closes this dialog box.

Cancel

Nullifies settings and closes this dialog box.

Help

Displays the help for this dialog box.