This section describes coverage measurements that are conducted using the coverage facility.
There are several kinds of coverage measurement methods. Of these, CS+ performs, in areas designated below, a code coverage measurement of fetch-related operations on source lines and functions (C0 coverage) and a data coverage measurement of access-related operations on variables.
The areas in which CS+ performs coverage measurements are as follows:
C0 coverage refers to an instruction coverage rate (statement coverage). |
In the E20 [RX71M, RX65x, and RX64M Groups], this function cannot be used together with the trace function or real-time RAM monitor function. |
In the E20 (JTAG) [RX71M, RX65x, and RX64M Group], if you connect the emulator by using hot plug-in, the coverage measurement function is not available. |