2.5 Options

This section describes the options for the RX family C/C++ compiler in each processing phase.

Compile phase: Refer to 2.5.1 Compile Options.

Assembly phase: Refer to 2.5.2 Assembler Command Options.

Link phase: Refer to 2.5.3 Optimizing Linkage Editor (rlink) Options.

Library generation phase: Refer to 2.5.4 Library Generator Options.