2. FUNCTIONS

The update feature updates installed tools and help to their latest versions.

It acquires information about the latest versions via the Internet, and then downloads and installs them.

There are three ways of updating tools and help files: manually following instructions on the screen, automatically checking for updates in accord with the settings made by the user, and automatically completing the entire process up to downloading.

Caution

When you use the update feature, the host machine must have a connection to the Internet. Also note that an authentication dialog box for the proxy server may appear when the CS+ Update Manager window is being opened. In such a case, enter the user name and password for the proxy server.