Everything

 

-error_file


This option outputs error messages to a file.

[Specification format]

-error_file=file

 

-

Interpretation when omitted

Error messages are output to only the standard error output.

[Detailed description]

-

This option outputs error messages to the standard error output and file file.

-

If file already exists, it will be overwritten.

-

An error will occur if file is omitted.

[Example of use]

-

To output error messages to the standard error output and file "err", describe as:

>asrl -error_file=err -dev=dr5f100pj.dvf main.asm