Everything

 

-BYte_count


This option specifies the maximum byte count for a data record.

[Specification format]

-BYte_count=num

 

-

Interpretation when omitted

When the -form=hexadecimal option is specified, an Intel HEX file is generated assuming that the maximum byte count is "0xFF".

When the -form=stype option is specified, a Motorola S-record file is generated assuming that the maximum byte count is "0x10".

[Detailed description]

-

This option is used to specify the length of data records in Intel HEX files or Motorola S-record files to be generated.

-

Values from 01 to FF (hexadecimal) are specifiable for Intel HEX files.

-

The following ranges of values are specifiable for Motorola S-record files.

-

S1 records: 01 to FC (hexadecimal)

-

S2 records: 01 to FB (hexadecimal)

-

S3 records: 01 to FA (hexadecimal)

[Example of use]

-

To specify 0x10 as the maximum byte count for a data record, describe as:

>rlink a.obj b.obj -form=hexadecimal -byte_count=10

[Remark]

-

When the -form={hexadecimal|stype} option is not specified, this option will be invalid.