Everything
10.3 MESSAGE TYPES

Table 10.1

Message Type (CC-RX (V2.00.00 or higher))

Message Type

Description

C

Internal error : Processing is aborted.

No output objects are generated.

E

Error : Processingn is aborted if a set number of errors occur.

No output objects are generated.

F

Fatal error : Processing is aaborted.

No output objects are generated.

M

Information : Informational message.

Check the message and continue the process.

W

Warning : Processing continues.

Output objects are generated (They might not be what the user intended).