F0511128 |
[Message] |
Library file "file-name" is not found. |
F0512003 |
[Message] |
Toomany errors. |
F0520003 |
[Message] |
#include file "file" includes itself. |
[Explanation] |
#include file "file" includes itself. Correct the error. |
F0520004 |
[Message] |
Out of memory. |
[Action by User] |
Out of memory. Close other applications, and perform the compile again. |
F0520005 |
[Message] |
Could not open source file "file". |
F0520013 |
[Message] |
Expected a file name. |
F0520016 |
[Message] |
"file" is not a valid source file name. |
F0520035 |
[Message] |
#error directive: character string |
[Explanation] |
There is an "#error" directive in the source file. |
F0520143 |
[Message] |
Program too large or complicated to compile. |
F0520163 |
[Message] |
Could not open temporary file xxx. |
F0520164 |
[Message] |
Name of directory for temporary files is too long (xxx). |
F0520182 |
[Message] |
Could not open source file xxx (no directories in search list). |
F0520189 |
[Message] |
Error while writing "file" file. |
F0520190 |
[Message] |
Invalid intermediate language file. |
F0520219 |
[Message] |
Error while deleting file "file". |
F0520542 |
[Message] |
Could not create instantiation request file name. |
F0520563 |
[Message] |
Invalid preprocessor output file. |
F0520564 |
[Message] |
Cannot open preprocessor output file. |
F0520571 |
[Message] |
Invalid option: option |
F0520641 |
[Message] |
xxx is not a valid directory. |
F0520642 |
[Message] |
Cannot build temporary file name. |
F0520869 |
[Message] |
Could not set locale xxx to allow processing of multibyte characters. |
F0520919 |
[Message] |
Invalid output file: xxx |
F0520920 |
[Message] |
Cannot open output file: xxx |
F0520926 |
[Message] |
Cannot open definition list file: xxx |
F0521083 |
[Message] |
Exported template file xxx is corrupted. |
F0521151 |
[Message] |
Mangled name is too long. |
F0521335 |
[Message] |
Cannot open predefined macro file: xxx |
F0521336 |
[Message] |
Invalid predefined macro entry at line line: line2 |
F0521337 |
[Message] |
Invalid macro mode name xxx. |
F0521338 |
[Message] |
Incompatible redefinition of predefined macro xxx. |
F0523029 |
[Message] |
Cannot open rule file |
[Explanation] |
The file specified in the -misra2004="file name" or -misra2012="file name" option cannot be opened. |
F0523030 |
[Message] |
Incorrect description "file name" in rule file |
[Explanation] |
The file specified in the -misra2004="file name" or -misra2012="file name" option includes illegal code. |
F0523031 |
[Message] |
Rule rule number is unsupported |
[Explanation] |
The number of a rule that is not supported was specified. |
F0523073 |
[Message] |
"instruction-set architecture name" does not support this intrinsic function. |
[Explanation] |
The specified intrinsic function is not supported. Check the -isa option setting. |
F0523088 |
[Message] |
Bit position is out of range. |
F0523129 |
[Message] |
The "option name" option is necessary for use of "function". |
[Explanation] |
The option must be specified to use this function. |
F0523300 |
[Message] |
Cannot open internal file. |
[Explanation] |
An intermediate file internally generated by the compiler cannot be opened. |
F0523301 |
[Message] |
Cannot close internal file. |
[Explanation] |
An intermediate file internally generated by the compiler cannot be closed. |
F0523302 |
[Message] |
Cannot write internal file. |
[Explanation] |
An error occurred while an intermediate file was being written to. |
F0530320 |
[Message] |
Duplicate symbol "symbol name". |
F0530800 |
[Message] |
Type of symbol "symbol-name" differs between files. |
F0530808 |
[Message] |
Alignment of variable "variable-name" differs between files. |
F0530810 |
[Message] |
#pragma directive for symbol "symbol-name" differs between files. |
F0533021 |
[Message] |
Out of memory. |
[Explanation] |
Memory is insufficient. |
[Action by User] |
Close other applications and recompile the program. |
F0533300 |
[Message] |
Cannot open an intermediate file. |
[Explanation] |
A temporary file that was internally generated by the compiler cannot be opened. |
F0533301 |
[Message] |
Cannot close an intermediate file. |
[Explanation] |
A temporary file that was internally generated by the compiler cannot be closed. |
F0533302 |
[Message] |
Cannot read an intermediate file. |
[Explanation] |
An error occurred during reading of a temporary file. |
F0533303 |
[Message] |
Cannot write to an intermediate file. |
[Explanation] |
An error occurred during writing of a temporary file. |
F0533306 |
[Message] |
Compilation was interrupted. |
[Explanation] |
During compilation, an interrupt due to entry of the Cntl + C key combination was detected. |
F0533330 |
[Message] |
Cannot open an intermediate file. |
[Explanation] |
A temporary file that was internally generated by the compiler cannot be opened. |
F0540027 |
[Message] |
Cannot read file "file-name". |
F0540204 |
[Message] |
Illegal stack access. |
[Explanation] |
Attempted usage of the stack by a function has exceeded 2 Gbytes. |
F0540300 |
[Message] |
Cannot open an intermediate file. |
[Explanation] |
A temporary file that was internally generated by the compiler cannot be opened. |
F0540301 |
[Message] |
Cannot close an intermediate file. |
[Explanation] |
A temporary file that was internally generated by the compiler cannot be closed. |
F0540302 |
[Message] |
Cannot read an intermediate file. |
[Explanation] |
An error occurred during reading of a temporary file. |
F0540303 |
[Message] |
Cannot write to an intermediate file. |
[Explanation] |
An error occurred during writing of a temporary file. |
F0540400 |
[Message] |
Different parameters are set for the same #pramga "identifier". |
F0544302 |
[Message] |
Cannot read an intermediate file. |
[Explanation] |
An error occurred while an intermediate file was being read. |
F0544802 |
[Message] |
The value of the parameter for the in-line function is outside the defined range. |
[Explanation] |
The value of the parameter for the inline function is outside the supported range. |
F0553000 |
[Message] |
Can't create file 'filename'. |
[Explanation] |
The filename file cannot be generated. |
[Action by User] |
Check the directory capacity. |
F0553001 |
[Message] |
Can't open file 'filename'. |
[Explanation] |
The filename file cannot be opened. |
[Action by User] |
Check the file name. |
F0553002 |
[Message] |
Can't write file 'filename'. |
[Explanation] |
The filename file cannot be written to. |
[Action by User] |
Check the permission of the file. |
F0553003 |
[Message] |
Can't read file 'filename'. |
[Explanation] |
The filename file cannot be read. |
[Action by User] |
Check the permission of the file. |
F0553004 |
[Message] |
Can't create Temporary file. |
[Explanation] |
Temporary file cannot be generated. |
[Action by User] |
Specify a directory in environment variable TMP_RX so that a temporary file will be created in some place other than the current directory. |
F0553005 |
[Message] |
Can't open Temporary file. |
[Explanation] |
The temporary file cannot be opened. |
[Action by User] |
Check the directory specified in TMP_RX. |
F0553006 |
[Message] |
Can't read Temporary file. |
[Explanation] |
The temporary file cannot be read. |
[Action by User] |
Check the directory specified in TMP_RX. |
F0553007 |
[Message] |
Can't write Temporary file. |
[Explanation] |
The temporary file cannot be written to. |
[Action by User] |
Check the directory specified in TMP_RX. |
F0553008 |
[Message] |
Illegal file name 'filename'. |
[Explanation] |
The file name is illegal. |
[Action by User] |
Specify a file name that conforms to file name description rules. |
F0553016 |
[Message] |
Lacking cpu specification. |
[Explanation] |
No CPU type is specified. |
[Action by User] |
Specify the CPU type by the cpuoption or environment variable CPU_RX. |
F0553100 |
[Message] |
Command line is too long. |
[Explanation] |
The command line has too many characters. |
[Action by User] |
Re-input the command. |
F0553101 |
[Message] |
Invalid option 'xx' is used. |
[Explanation] |
An invalid command option xx is used. |
[Action by User] |
The specified option is nonexistent. Re-input the command correctly. |
F0553102 |
[Message] |
Ignore option 'xx'. |
[Explanation] |
An invalid option is specified. |
F0553103 |
[Message] |
Option 'xx' is not appropriate. |
[Explanation] |
Command option xx is written incorrectly. |
[Action by User] |
Specify the command option correctly again. |
F0553104 |
[Message] |
No input files specified. |
[Explanation] |
No input file is specified. |
[Action by User] |
Specify an input file. |
F0553105 |
[Message] |
Source files number exceed 80. |
[Explanation] |
The number of source files exceeds 80. |
[Action by User] |
Execute assembling separately in two or more operations. |
F0553106 |
[Message] |
Lacking cpu specification. |
[Explanation] |
No CPU type is specified. |
[Action by User] |
Specify the CPU type by the cpuoption or environment variable CPU_RX. |
F0553110 |
[Message] |
Multiple register base/fint_register. |
[Explanation] |
A single register is specified by the baseand fint_registeroptions. |
F0553111 |
[Message] |
Multiple register base/pid. |
[Explanation] |
A single register is specified by the baseand pidoptions. |
F0553112 |
[Message] |
Multiple register base/nouse_pid_register. |
[Explanation] |
A single register is specified by the baseand nouse_pid_registeroptions. |
F0553113 |
[Message] |
Neither isa nor cpu is specified |
F0553114 |
[Message] |
Both '-isa' option and '-cpu' option are specified |
F0553115 |
[Message] |
The '-cpu' option and the '-fpu' option are inconsistent |
F0553200 |
[Message] |
Error occurred in executing 'xxx'. |
[Explanation] |
An error occurred when executing xxx. |
[Action by User] |
Rerun asrx. |
F0553201 |
[Message] |
Not enough memory. |
[Explanation] |
Memory is insufficient. |
[Action by User] |
Divide the file and re-run. Orincrease the memory capacity. |
F0553202 |
[Message] |
Can't find work dir. |
[Explanation] |
The work directory is not found. |
[Action by User] |
Make sure that the setting of environment variable TMP_RX is correct. |
F0563000 |
[Message] |
No input file |
[Explanation] |
There is no input file. |
F0563001 |
[Message] |
No module in library |
[Explanation] |
There are no modules in the library. |
F0563002 |
[Message] |
Option "option1" is ineffective without option "option2" |
[Explanation] |
The option option 1 requires that the option option 2 be specified. |
F0563003 |
[Message] |
Illegal file format "file" |
F0563004 |
[Message] |
Invalid inter-module optimization information type in "file" |
[Explanation] |
The file contains an unsupported inter-module optimization information type. |
[Action by User] |
Check if the compiler and assembler versions are correct. |
F0563020 |
[Message] |
No cpu information in input files |
[Explanation] |
The CPU type cannot be identified from the input file. |
[Action by User] |
Check that the binary file is specified with the -binary option and the .obj or .rel files to be linked together exist. |
F0563100 |
[Message] |
Section address overflow out of range : "section" |
[Explanation] |
The address of section exceeded the area available. |
[Action by User] |
Change the address specified by the start option.
For details of the address space, refer to the hardware manual of the target CPU. |
F0563102 |
[Message] |
Section contents overlap in absolute section "section" in "file" |
[Explanation] |
Data addresses overlap within an absolute address section. |
[Action by User] |
Modify the source program. |
F0563103 |
[Message] |
Section size overflow : "section" |
[Explanation] |
Section "section" has exceeded the usable size. |
F0563110 |
[Message] |
Illegal cpu type "cpu type" in "file" |
[Explanation] |
A file with a different cpu type was input. |
F0563111 |
[Message] |
Illegal encode type "endian type" in "file" |
[Explanation] |
A file with a different endian type was input. |
F0563112 |
[Message] |
Invalid relocation type in "file" |
[Explanation] |
There is an unsupported relocation type in file. |
[Action by User] |
Ensure the compiler and assembler versions are correct. |
F0563115 |
[Message] |
Cpu type in "file" is not supported |
[Explanation] |
The CPU type specified in "file" is not supported. Check if the input file is correct. |
F0563120 |
[Message] |
Illegal size of the absolute code section : "section" in "file" |
[Explanation] |
Absolute-addressing section section in file has an illegal size. |
F0563150 |
[Message] |
Multiple files cannot be specified while processing "process" |
F0563200 |
[Message] |
Too many sections |
[Explanation] |
The number of sections exceeded the translation limit. It may be possible to eliminate this problem by specifying multiple file output. |
F0563201 |
[Message] |
Too many symbols |
[Explanation] |
The number of symbols exceeded the translation limit. It may be possible to eliminate this problem by specifying multiple file output. |
F0563202 |
[Message] |
Too many modules |
[Explanation] |
The number of modules exceeded the translation limit. |
[Action by User] |
Divide the library. |
F0563203 |
[Message] |
Reserved module name "rlink_generates" |
[Explanation] |
rlink_generates_** (** is a value from 01 to 99) is a reserved name used by the optimizing linkage editor. It is used as an .obj or .rel file name or a module name within a library. |
[Action by User] |
Modify the name if it is used as a file name or a module name within a library. |
F0563204 |
[Message] |
Reserved section name "$sss_fetch" |
[Explanation] |
sss_fetch** (sss is any string, and ** is a value from 01 to 99) is a reserved name used by the optimizing linkage editor. |
[Action by User] |
Change the symbol name or section name. |
F0563300 |
[Message] |
Cannot open file : "file" |
[Explanation] |
file cannot be opened. |
[Action by User] |
Check whether the file name and access rights are correct. |
F0563301 |
[Message] |
Cannot close file : "file" |
[Explanation] |
file cannot be closed. There may be insufficient disk space. |
F0563302 |
[Message] |
Cannot write file : "file" |
[Explanation] |
Writing to file is not possible. There may be insufficient disk space. |
F0563303 |
[Message] |
Cannot read file : "file" |
[Explanation] |
file cannot be read. An empty file may have been input, or there may be insufficient disk space. |
F0563310 |
[Message] |
Cannot open temporary file |
[Explanation] |
A temporary file cannot be opened. |
[Action by User] |
Check to ensure the HLNK_TMP specification is correct, or there may be insufficient disk space. |
F0563314 |
[Message] |
Cannot delete temporary file |
[Explanation] |
A temporary file cannot be deleted. There may be insufficient disk space. |
F0563320 |
[Message] |
Memory overflow |
[Explanation] |
There is no more space in the usable memory within the linker. |
[Action by User] |
Increase the amount of memory available. |
F0563400 |
[Message] |
Cannot execute "load module" |
[Explanation] |
load module cannot be executed. |
[Action by User] |
Check whether the path for load module is set correctly. |
F0563410 |
[Message] |
Interrupt by user |
[Explanation] |
An interrupt generated by (Ctrl) + C keys from a standard input terminal was detected. |
F0563420 |
[Message] |
Error occurred in "load module" |
[Explanation] |
An error occurred while executing load module. |
F0563430 |
[Message] |
The total section size exceeded the limit of the evaluation version of version. Please consider purchasing the product. |
F0563431 |
[Message] |
Incorrect device type, object file mismatch. |
F0563600 |
[Message] |
Option "option" requires parameter |
F0563601 |
[Message] |
Invalid parameter specified in option "option" : "parameter" |
F0578200 |
[Message] |
memory allocation fault |
[Explanation] |
Not enough memory. |
F0578201 |
[Message] |
bad key character - use [dm(a|b)qr(a|b|u)txV] |
[Explanation] |
character cannot be specified as a key. |
F0578202 |
[Message] |
bad option character - use [cv] |
[Explanation] |
character cannot be specified as an option. |
F0578203 |
[Message] |
bad option string |
[Explanation] |
string cannot be specified as an option. |
F0578204 |
[Message] |
can not create file file |
[Explanation] |
Could not create file file. |
F0578205 |
[Message] |
file name name... is too long - limit is number |
[Explanation] |
File name name is too long. The maximum value is number1. |
F0578206 |
[Message] |
can not open file file |
[Explanation] |
Could not open file file. |
F0578207 |
[Message] |
can not close file file |
[Explanation] |
Could not close file file. |
F0578208 |
[Message] |
can not read file file |
[Explanation] |
Cannot read from file file. |
F0578209 |
[Message] |
can not write file file |
[Explanation] |
Cannot write to file file. |
F0578210 |
[Message] |
can not seek file file |
[Explanation] |
Cannot seek in file file. |
F0578212 |
[Message] |
can not nest command file file |
[Explanation] |
Command file file is nested. Nesting is not allowed. |
F0578213 |
[Message] |
file is not library file |
[Explanation] |
file is not a library file. |
F0578214 |
[Message] |
malformed library file file |
[Explanation] |
Library file file could be corrupt. |
F0578215 |
[Message] |
can not find member member |
[Explanation] |
Member member not found in library file. |
F0578216 |
[Message] |
symbol table limit error file (number1) - limit is number2 |
[Explanation] |
The number of symbols number1 in library file file exceeds the maximum limit. The maximum value is number2. |
F0578217 |
[Message] |
symbol table error file |
[Explanation] |
Failed to create a library file table for library file file. |
F0578218 |
[Message] |
string table error file |
[Explanation] |
The library string table for library file file could be corrupt. |
F0578219 |
[Message] |
file has no member |
[Explanation] |
There are no members in library file file. |
F0578220 |
[Message] |
version error file |
[Explanation] |
The version of the format of the specified file file is not supported by this librarian. |
F0578221 |
[Message] |
can not read library header file |
[Explanation] |
Cannot read header from library file file. |
F0593113 |
[Message] |
Neither isa nor cpu is specified |
F0593114 |
[Message] |
Both '-isa' option and '-cpu' option are specified |