Everything
2.2 Set the Columns to Display

The columns or marks displayed on the Editor panel can be set by selecting the toolbar items shown below.

Note that this setting applies to all of the Editor panels.

Columns

The following items are displayed to show or hide the columns or marks on the Editor panels.

Remove the check to hide the items (all the items are checked by default).

 

Line Number

Shows the line number, in the line number area.

Selection

Shows the mark that indicates the line modification status, in the line number area.

Out of date module indicator

Shows the mark that indicates the update status of the downloaded load module file, in the line number area.

Note that this item is enabled only when connected to the debug tool.

Coverage

Shows the coverage area.

Note that this item is enabled only when connected to the debug tool.

Address

Shows the address area.

Note that this item is enabled only when connected to the debug tool.

Op Code

Shows the code area.

Note that this item is enabled only when connected to the debug tool and the Mixed display mode is selected.

Label

Shows the label area.

Note that this item is enabled only when connected to the debug tool and the Mixed display mode is selected.

Event

Shows the event area.

Note that this item is enabled only when connected to the debug tool.

Main

Shows the main area.

Column Header

Shows the column header.