Everything

project.GetDeviceNameList


This function displays the list of the device names of the microcontroller.

[Specification format]

project.GetDeviceNameList(micomType, nickName = "")

[Argument(s)]

Argument

Description

micomType

Specify the microcontroller type of a new project.

The types that can be specified are shown below.

Type

Description

MicomType.RH850

Project for RH850

MicomType.RX

Project for RX

MicomType.V850

Project for V850

MicomType.RL78

Project for RL78

MicomType.K0R

Project for 78K0R

MicomType.K0

Project for 78K0

nickName

Specify the nickname of the microcontroller by a string (default: not specified).

Specify a character string displayed in the first layer of the [Using microcontroller] list in the Create Project dialog box that is used to create a new project.

[Return value]

List of device names

[Detailed description]

-

This function displays the list of the device names of the microcontroller specified by micomType.

-

When nickName is specified, only the names of the devices specified by nickName are displayed.

[Example of use]

>>>project.GetDeviceNameList(MicomType.RL78)
R5F10BAF
R5F10AGF
R5F10BAG
R5F10BGG
........
>>>devlist = project.GetDeviceNameList(MicomType.RL78, "RL78/F13 (ROM:128KB)")
R5F10BAG
R5F10BGG
........
>>>