Everything

csplus.is_debug_session_running


This function checkes the debug sesion is running or not.

[Specification format]

csplus.is_debug_session_running(session_id)

[Argument(s)]

Argument

Description

session_id

This argument is ignored in this version.

[Return value]

True if debug session is running, False if debug session is suspending.

[Detailed description]

-

If is_debug_session_running is called unsuccessfully, an exception will be thrown. In case of multicore device, only the first core is checked.

[Example of use]

>>> csplus.is_debug_session_running(session_id)
True
>>>