Everything

2.1 When Not Using RI600V4, RI600PX Configurator

The output format when not using the RI600V4, RI600PX Configurator is as follows.
(1) When the file name and line number information are included
 file-name (line-number) : message-type component-number message-number : message

(2) When the file name and line number information aren't included
 message-type component-number message-number : message

Remarks 1. Following contents are output as the continued character string.
message-type: 1 alphabetic character (C, E, F, M, W)
component-number: 11
message-number: 5 digits
2. See "CubeSuite+ Message" for details about the message-type, the component-number and the message-number.