Everything
 

Add Section dialog box

Modify Section dialog box

Add Overlay dialog box


These dialog boxes are used to set a section name when adding, modifying, or overlaying a section, respectively.

Figure A.5

Add Section Dialog Box

Figure A.6

Modify Section Dialog Box

Figure A.7

Add Overlay Dialog Box

 

The following items are explained here.

[How to open]

-

Add Section dialog box

-

On the Section Settings dialog box, select a section in the address-section area, and then click the [Add...] button.

-

Modify Section dialog box

-

On the Section Settings dialog box, select a section in the address-section area, and then click the [Modify...] button.

-

Add Overlay dialog box

-

On the Section Settings dialog box, click the [New Overlay...] button.

[Description of each area]

(1)

[Section name]

Specify the section name.

Directly enter the section name in the text box or select from the drop-down list.

The following characters can be used only: A-Z, a-z, 0-9, @, _, *, dot(.).

Wildcard characters (*) can also be used.

Note that numeric characters (0 to 9) and dot(.) cannot be used at the beginning of a section name.

The following reserved sections are set in the drop-down list.

.bss, .const, .data, .text

[Function buttons]

Button

Function

OK

-

Add Section dialog box

Closes this dialog box and adds the specified section to the address-section area in the Section Settings dialog box.

When there is no empty column in the section group (an address and the sections allocated to the address) where the specified section is to be included, a new section row is added to the bottom of the section group. When there is an empty column, the section is added there.

-

Modify Section dialog box

Closes this dialog box and replaces the section name selected in the address-section area in the Section Settings dialog box with the one specified.

-

Add Overlay dialog box

Closes this dialog box and adds the [Overlayn] column (n: number starting with "1") to the address-section area in the Section Settings dialog box.

Sets the specified section in the column that corresponds to the selected section group.

Cancel

Cancels the settings and closes this dialog box.

Help

Displays the help of this dialog box.