Everything
2.2 Speeding-up of Build

The build speed-up facilities of this build tool are described here.

 

There are the following types of build speed-up facilities.

Simultaneous build

Multiple files are simultaneously passed by a single call of the build command.

See "2.2.1Running simultaneous build" for details about simultaneous build.

Parallel build

Multiple build commands are executed in parallel.

See "2.2.2Running parallel build" for details about parallel build.