Everything
2.13 Estimate the Stack Capacity

To estimate the stack capacity, use Call Walker.

Call Walker performs a static analysis, and displays the symbols and their callers in a tree format, as well as stack information for each symbol (symbol name, attribute, address, size, stack size, and file name) in list format.

To start Call Walker, select [Tool] menu >> [Startup Stack Usage Tracer].

To exit from Call Walker, select Call Walker [File] menu >> [Exit].

See Call Walker [Help] menu >> [Help Topics] for Call Walker operations.