Everything
2.7.2 Display the result of disassembling

The result of disassembling the downloaded program (disassembled text) is displayed in the Disassemble panel below.

Select [View] menu >> [Disassemble] >> [Disassemble1 - 4].

The maximum of 4 Disassemble panels can be opened. Each panel is identified by the names "Disassemble1", "Disassemble2", "Disassemble3" and "Disassemble4" on the titlebar.

For details on the contents and function in each area, see the section for the Disassemble panel.

Figure 2.19

Display Result of Disassembling (Disassemble Panel)

Remark

You can set the scroll range of the vertical scroll bar on this panel via the Scroll Range Settings dialog box which is opened by clicking the button from [View] on the toolbar.

This section describes the following.

 

2.7.2.1 Change display mode

2.7.2.2 Change display format

2.7.2.3 Move to the specified address

2.7.2.4 Move to the symbol defined location

2.7.2.5 Save the disassembled text contents