Everything
2.12.3.1 Search for an I/O register

An I/O register can be searched for.

Specify the I/O register name to search with the text box in the search area (case-insensitive). You can either type character strings directly from the key board (up to 512 characters), or select one from the input history via the drop-down list (up to 10 items). Then, click either one of the following button.

 

Searches up for the I/O register name containing the string specified in the text box, and selects the I/O register that is found.

 

Searches down for the I/O register name containing the string specified in the text box, and selects the I/O register that is found.

Remark 1.

The hidden I/O register name being classified with a category can be searched (the category is opened and the I/O register is selected).

Remark 2.

After typing character strings to search, to press the [Enter] key is the same function as clicking the button, and to press the [Shift] + [Enter] key is the same function as clicking the button.