Everything
2.3.6 [COM Port]

Configure the operating environment on the Property panel below when using COM Port.

Figure 2.11

Example of Property Panel [COM Port]

 

Follow the steps below by selecting the corresponding tab on the Property panel.

 

[Connect Settings] tab

[Debug Tool Settings] tab

[Download File Settings] tab

[Hook Transaction Settings] tab