Renesas Electronics
top
CAUTIONS
Cautions Regarding Compiler
11.1 Cautions Regarding Compiler
This section explains the cautions regarding the compiler.
Previous Topic
CAUTIONS
Next Topic
Indirect reference of pointer
Table of Contents
Cautions Regarding Compiler
Indirect reference of pointer
Register access via pointer
Function calling
Data flash area
Function definitions in K&R format (formal parameters of _Bool type)
MISRA 2004 check (rule number 10.1)
Extended language specifications which needs the device file
Cautions Regarding Library and Startup
Cautions Regarding Assembler
Cautions Regarding Linker