Renesas Electronics
top
CAUTIONS
Cautions Regarding Linker
11.4 Cautions Regarding Linker
This section explains the cautions regarding the linker.
Previous Topic
An option depending on the order of specification of options
Next Topic
-strip option
Table of Contents
Cautions Regarding Compiler
Cautions Regarding Library and Startup
Cautions Regarding Assembler
Cautions Regarding Linker
-strip option
-memory option
Overwrite of variable/function information file
Allocation of sections
Variable/function information file that may cause a compile error