| 
 Parts Led Properties dialog box 
 | 
This property dialog box is used to set or change the pin connection information of LED, which are one of the connection parts in the I/O Panel window. 
A pin-connected LED displays the information output from the simulator through lit/unlit display in the Simulation mode. 
There are two types of LED display styles, figure and bitmap. These styles can be changed on the [[Style] tab]. 
Figure A.75  | Parts Led Properties Dialog Box: [LED Connection] Tab  | 
 
Figure A.76  | Parts Led Properties Dialog Box: [Style] Tab  | 
 
 
This section describes the following.
[How to open]
On the I/O Panel window, any one of the following:
-  | Double-click a part object "LED".  | 
 
-  | Select [Properties...] form the context menu on a part object "LED".  | 
 
-  | Select a part object "LED", and then select [Properties...] form the [View] menu.  | 
 
[[LED Connection] tab]
(1)  | Pin connection information setting area  | 
 
| 
 
Label 
 | 
 
This area is used to specify the part name. The part name input here is also displayed in the Parts List dialog box as the label. 
 | 
| 
 
Pin Name 
 | 
 
This area is used to specify the pin name to be connected (output pin). The connection pins can be specified either via direct input or through selection from the drop-down list. 
 | 
| 
 
Active Level 
 | 
 
The active state is selected with a option button, as follows: 
 | 
| 
 
LOW 
 | 
 
Sets the active level to LOW. 
 | 
| 
 
HIGH 
 | 
 
Sets the active level to HIGH (default).  
 | 
 
Remark  | For the pin names that can be specified, see the user's manual of the microcontroller that is used.  | 
 
[[Style] tab]
(1)  | Style information setting area  | 
 
| 
 
Figure 
 | 
 
Select this option button to display the LED with the following specified figure. 
 | 
| 
 
Shape 
 | 
 
Select the figure shape. Two shapes can be selected: rectangle and ellipse.  
 | 
| 
 
shadow 
 | 
 
Cannot be selected. 
 | 
| 
 
Line 
 | 
 
Specify and change the figure line, as follows. 
You can change the color of figure line by clicking the pull-down button.  
 | 
| 
 
Thickness 
 | 
 
Specifies the line thickness.  
Specification is made either using a spin button or through direct input.  
A value from 1 to 100 can be specified.  
 | 
| 
 
Active 
 | 
 
Specifies the color of the line during active display. 
 | 
| 
 
Inactive 
 | 
 
Specifies the color of the line during inactive display. 
 | 
| 
 
Fill up 
 | 
 
Specify and change the figure filling, as follows. 
You can change the color of figure filling by clicking the pull-down button.  
 | 
| 
 
Active 
 | 
 
Specifies the fill color during active display. 
 | 
| 
 
Inactive 
 | 
 
Specifies the fill color during inactive display. 
 | 
| 
 
Bitmap 
 | 
 
Select this option button to display the LED with the following specified bitmap (default). 
 | 
| 
 
Selection list 
 | 
 
Select a bitmap to be used from the selection list.  
The selectable bitmaps appear in the selection list. 
 | 
| 
 
[Add] button 
 | 
 
Opens the Entry Bitmap dialog box below to add a new bitmap to the selection list.  
The bitmap file to be added can be specified either through file selection using the [...] button, or through direct input. 
 | 
| 
 
[Delete] button 
 | 
 
Deletes the currently selected bitmap from the selection list. 
Note that only the bitmap that have been added by user can be deleted. 
 | 
 
This area displays the style of the LED currently being specified.
[Function buttons]
| 
 | 
 | 
| 
 
OK 
 | 
 
Validates the settings and closes this dialog box. 
 | 
| 
 
Cancel 
 | 
 
Cancels the settings and closes this dialog box.  
 | 
| 
 
Apply 
 | 
 
Cannot be selected. 
 | 
| 
 
Help 
 | 
 
Displays the help for this dialog box.  
 | 
 
[Operation]
In the Simulation mode, the output status (active/inactive) of the connected pins is displayed in real-time using two types of bitmaps or figures. 
Figure A.77  | Connected Parts Display Example (LED)  |