| 
 Object Properties dialog box 
 | 
This property dialog box is used to set or change the connection information fed to the pins of figure object (including text and bitmap) of the I/O Panel window. 
Show/hide can be switched for each pin-connected object by the output status of the connected pins in the Simulation mode. 
The default status of each signal is active HIGH. Display styles can be changed on the [[Style] tab].
Figure A.88  | Object Properties Dialog Box: [Object Connection] Tab  | 
 
Figure A.89  | Object Properties Dialog Box: [Style] Tab  | 
 
 
This section describes the following.
[How to open]
On the I/O Panel window, any one of the following:
-  | Double-click a figure object.  | 
 
-  | Select [Properties...] form the context menu on a figure object.  | 
 
-  | Select a figure object, and then select [Properties...] form the [View] menu.  | 
 
[[Object Connection] tab]
(1)  | Pin connection information setting area  | 
 
| 
 
Pin Connect 
 | 
 
Select the method for connecting objects and output pins by clicking the corresponding option buttons, and specify the output pin name. 
As a result of the connection, figure display is switched by the ON/OFF status of the connected output pin. 
 | 
| 
 
No Connection 
 | 
 
The object and pin are not connected (default).  
Objects not connected to pins are always in the displayed status.  
 | 
| 
 
Static Connection 
 | 
 
Connects the figure to 1 output pin. 
The connection pin can be specified in [Pin Name] either via direct input or through selection from the drop-down list. During simulation, the object is displayed when the specified output signal data is active. 
 | 
| 
 
Dynamic Connection 
 | 
 
Connects the figure to 2 output pins. 
The connection pin can be specified in [Pin Name1] and [Pin Name2] either via direct input or through selection from the drop-down list. During simulation, the object is displayed when the specified output signal 1 data and the specified output signal 2 data are both active.  
 | 
| 
 
Active Level 
 | 
 
The common active status of each output signal can be selected from the option buttons.  
 | 
| 
 
LOW 
 | 
 
Sets the active level to LOW. 
 | 
| 
 
HIGH 
 | 
 
Sets the active level to HIGH (default).  
 | 
 
Remark  | For the pin names that can be specified, see the user's manual of the microcontroller that is used.  | 
 
[[Style] tab]
(1)  | Style information setting area  | 
 
| 
 
Fill up 
 | 
 
Specifies and changes settings related to each object fillingNote, as follows: 
The area to be filled differs according to the object.  
-  | Rectangle, Ellipse, Rounded Rectangle 
Inside area enclosed by contour lines   |  
  
-  | Polygon 
Inside area enclosed by lines linking apexes   |  
  
-  | Bitmap 
Inside figure drawing area   |  
  
 | 
| 
 
Color 
 | 
 
Specifies and changes settings of color  
You can change the color by clicking the pull-down button.  
 | 
| 
 
Line 
 | 
 
This area is used to perform settings and changes related to the lines of objects.  
The definition of line for each type of object is provided below. 
-  | Line 
All areas of the object   |  
  
-  | Rectangle, Ellipse, Rounded Rectangle 
Contour line of the figure   |  
  
-  | Polygon 
Lines that link the apexes of the polygon   |  
  
-  | Text 
Contour lines of the text box  |  
  
-  | Bitmap 
Contour lines of figure drawing area   |  
  
 | 
| 
 
Color 
 | 
 
Specifies and changes the line color. 
You can change the color by clicking the pull-down button.  
 | 
| 
 
Dotted/Solid 
 | 
 
Specifies and changes line shapes (dotted line/solid line).  
The desired line shape can be selected from the drop-down list.  
Note that this item can be changed only when [Thickness] is set to "1". 
 | 
| 
 
Thickness 
 | 
 
Specifies and changes the line thickness.  
The desired line thickness can be specified either via direct input or through selection from the spin button. 
A value in the range of 1 to 100 (decimal) can be specified. 
 | 
 
Note  | At this time, if the object that have been pasted from a bitmap file, it becomes invisible.  | 
 
[Function buttons]
| 
 | 
 | 
| 
 
OK 
 | 
 
Validates the settings and closes this dialog box. 
 | 
| 
 
Cancel 
 | 
 
Cancels the settings and closes this dialog box.  
 | 
| 
 
Apply 
 | 
 
Cannot be selected. 
 | 
| 
 
Help 
 | 
 
Displays the help for this dialog box.  
 |