Renesas Electronics
top
Build Tool Operation
FUNCTIONS
Overview
2.1 Overview
This section describes how to create a load module and user library.
Previous Topic
FUNCTIONS
Next Topic
Create a load module
Table of Contents
Overview
Create a load module
Create a user library
Convert a CA78K0R project into a CC-RL project
Speeding-up of Build
Set the Type of the Output File
Set Compile Options
Set Assemble Options
Set Link Options
Set Hex Output Options
Set Create Library Options
Set Build Options Separately
Efficiently Allocate Variables and Functions
Automatically Update the I/O Header File
Estimate the Stack Capacity