2.10 Set Build Options Separately

Build options are set at the project or file level.

 

Project level: See "2.10.1 Set build options at the project level"

File level: See "2.10.2 Set build options at the file level"