r_csigm_callback_sendend


Performs processing in response to the CSIG communication interrupt.

Remark

This API function is called as the callback routine of interrupt process r_csigm_interrupt_send corresponding to the CSIG communication interrupt.

Syntax

void    r_csigm_callback_sendend ( void );

Remark

m is the channel number.

Argument(s)

None.

Return value

None.