Performs processing in response to the CSIG error interrupt.
Remark | This API function is called as the callback routine of interrupt process r_csigm_interrupt_errorcorresponding to the CSIG error interrupt. |
Syntax
#include "r_cg_macrodriver.h"
void r_csigm_callback_error ( uint8_t err_type );
|
Remark | m is the channel number. |
Argument(s)
|
|
|
|
|
|
uint8_t err_type;
|
Trigger for CSIG error interrupt
0000x0x1B Overrun error
0000x01xB Parity error
000010xxB Data consistency check error
|
Return value
None.