Renesas Electronics
r_csihm_callback_receiveend
Performs processing in response to the CSIH reception interrupt.
Remark
This API function is called as the callback routine of interrupt process r_csihm_interrupt_receive corresponding to the CSIH reception interrupt.
Syntax
void r_csihm_callback_receiveend ( void );
m is the channel number.
Argument(s)
None.
Return value