Renesas Electronics
r_csihm_callback_sendend
Performs processing in response to the CSIH communication interrupt.
Remark
This API function is called as the callback routine of interrupt process r_csihm_interrupt_send corresponding to the CSIH communication interrupt.
Syntax
void r_csihm_callback_sendend ( void );
m is the channel number.
Argument(s)
None.
Return value