Halts the clock supplied to the oscillation stop detector.
Remark | Calling this API function changes the oscillation stop detector to reset status.
For this reason, writes to the control registers after this API function is called are ignored. |
[Syntax]
void R_OSDC_Set_PowerOff ( void );
|
[Argument(s)]
None.
[Return value]
None.