3.2.42
Oscillation stop detector
Below is a list of API functions output by the Code Generator for oscillation stop detector use.
Table 3.42 | API Functions: [Oscillation Stop Detector] |
|
|
|
|
R_OSDC_Create
|
Performs initialization necessary to control the oscillation stop detector.
|
|
R_OSDC_Create_UserInit
|
Performs user-defined initialization relating to the oscillation stop detector.
|
|
r_osdc_interrupt
|
Performs processing in response to the oscillation stop detection interrupt INTOSDC.
|
|
R_OSDC_Start
|
Enables operation of oscillation stop detector.
|
|
R_OSDC_Stop
|
Disables operation of oscillation stop detector.
|
|
R_OSDC_Set_PowerOff
|
Halts the clock supplied to the oscillation stop detector.
|
|
R_OSDC_Reset
|
Reset the oscillation stop detector.
|