| 
 R_TMR_KBm_BatchOverwriteRequestOn 
 | 
Enables batch overwriting of the compare register.
Remark  | The timing for batch-overwriting the content of the compare register is when a count value and a value set in the compare register are matched or an external trigger is generated after calling this API function.  | 
 
[Syntax]
void    R_TMR_KBm_BatchOverwriteRequestOn ( void ); 
 | 
 
Remark  | m is the unit number.  | 
 
[Argument(s)]
None.
[Return value]
None.