Renesas Electronics
Below is a list of API functions output by the Code Generator for 16-bit timer KC0 use.
Table 3.11
API Functions: [16-bit Timer KC0]
API Function Name
Function
R_TMR_KC0_Create
Performs initialization necessary to control the 16-bit timer KC0.
R_TMR_KC0_Create_UserInit
Performs user-defined initialization relating to the 16-bit timer KC0.
r_tmr_kc0_interrupt
Performs processing in response to the timer interrupt.
R_TMR_KC0_Start
Starts the count for 16-bit timer KC0.
R_TMR_KC0_Stop
Ends the count for 16-bit timer KC0.
R_TMR_KC0_Set_PowerOff
Halts the clock supplied to the 16-bit timer KC0.