Renesas Electronics
R_TMR_RG0_Create_UserInit
Performs user-defined initialization relating to the 16-bit timer RG0.
Remark
This API function is called as the R_TMR_RG0_Create callback routine.
[Syntax]
void R_TMR_RG0_Create_UserInit ( void );
[Argument(s)]
None.
[Return value]