3.2.8 Timer RG

Below is a list of API functions output by the Code Generator for timer RG use.

Table 3.8

API Functions: [Timer RG]

API Function Name

Function

R_TMR_RG0_Create

Performs initialization necessary to control the 16-bit timer RG0.

R_TMR_RG0_Create_UserInit

Performs user-defined initialization relating to the 16-bit timer RG0.

r_tmr_rg0_interrupt

Performs processing in response to the timer interrupt.

R_TMR_RG0_Start

Starts the count for 16-bit timer RG0.

R_TMR_RG0_Stop

Ends the count for 16-bit timer RG0.

R_TMR_RG0_Set_PowerOff

Halts the clock supplied to the 16-bit timer RG0.

R_TMR_RG0_Get_PulseWidth

Reads the pulse width of the 16-bit timer RG0.