R_LPC_ChangeOperationPowerControl


Changes the operating power control mode of the MCU.

[Syntax]

#include    "r_cg_macrodriver.h"
#include    "r_cg_lpc.h"
MD_STATUS   R_LPC_ChangeOperationPowerControl ( operaring_mode_t mode );

[Argument(s)]

I/O

Argument

Description

I

operating_mode_t  mode;

Operating power control mode type

HIGH_SPEED: High-speed operating mode

MIDDLE_SPEED: Middle-speed operating mode

LOW_SPEED: Low-speed operating mode

[Return value]

Macro

Description

MD_OK

Normal completion

MD_ERROR1

Change to the low-speed operating mode ended abnormally.

MD_ERROR2

Change to the middle-speed operating mode is ended abnormally.

MD_ARGERROR

Invalid argument mode specification