R_LPC_DeepSleep


Transits the low power consumption mode of the MCU to the deep sleep mode.

[Syntax]

#include    "r_cg_macrodriver.h"
MD_STATUS   R_LPC_DeepSleep ( void );

[Argument(s)]

None.

[Return value]

Macro

Description

MD_OK

Normal completion

MD_ERROR1

Exit with error (abend)