R_SCIn_IIC_StartCondition


Sends the start bit.

Remark

This API function is called as the internal function of R_SCIn_IIC_Master_Send and R_SCIn_IIC_Master_Receive.

[Syntax]

void    R_SCIn_IIC_StartCondition ( void );

Remark

n is the channel number.

[Argument(s)]

None.

[Return value]

None.