Renesas Electronics
R_SCIn_Create_UserInit
Performs user-defined initialization related to the serial communications interface.
Remark
This API function is called as the R_SCIn_Create callback routine.
[Syntax]
void R_SCIn_Create_UserInit ( void );
n is the channel number.
[Argument(s)]
None.
[Return value]