1.2 Special Features

CC-RH is equipped with the following special features.

(1)

Language specifications in accordance with ANSI standard

The C language specifications conform to the ANSI standard.

(2)

Advanced optimization

Advanced optimization is used, applying global program optimization as well as conventional optimization.

This yields smaller, faster code, and also reduces build times.

(3)

High portability

The program supports porting programs from the existing SuperH RISC engine C/C++ compiler.

In addition, the industry-standard DWARF2 format is used for debugging information.

(4)

Multifunctional

Static analysis and other functionality is provided via linking between CS+.