There are two variants of this license - the Professional Edition and the Standard Edition. The usable options are limited
For the usable options in the Professional Edition, see "Table 2.2 Compile Options" or the description for each option.
The functions of the Professional Edition can be used with the free evaluation license within the evaluation period.
There are two license types, and the license is confirmed with the following priority.
If a floating license is available, a license request is made to the license even in the case a free evaluation license
is within the evaluation period.
When none of the following conditions are met at linkage, the license is regarded as a free evaluation one and the total
size of linked objects is restricted.
The evaluation period of 60 days has not passed since the first time the optimizing linker was invoked. |
The size limitation specifies that for a section whose section type is PROGBITS and whose section attribute is allocate,
the total size of the section should be up to 256 Kbytes. When the size exceeds 256 Kbytes, an error will occur.
The version sign of the optimizing linker is W when operating as a free evaluation version and is V when operating as a
Output examples are given below.