-FSymbol


This option outputs external defined symbols to the symbol address file.

[Specification format]

-FSymbol=section[,section]...

 

-

Interpretation when omitted

None

[Detailed description]

-

This option outputs the external defined symbols in section section to a file (symbol address file) in the form of assembler directives.
The file name is "output file name.fsy".

[Example of use]

-

To output the external defined symbols in sections "sct2" and "sct3" to symbol address file "test.fsy", describe as:

>rlink a.obj b.obj -fsymbol=sct2,stc3 -output=test.abs

 

The output example of symbol address file "test.fsy" is shown below.

;RENESAS OPTIMIZING LINKER GENERATED FILE xxxx.xx.xx
;fsymbol = sct2,sct3
 
;SECTION NAME = sct2
    .public _f
_f .equ 0x0
    .public _g
_g .equ 0x16
;SECTION NAME = sct3
    .public _main
_main .equ 0x20

[Remark]

-

If the -form={object|relocate|library} option or -strip option is specified, this option will be invalid.