-ALIGNED_SECTION


This option changes the number of alignment of the section to 16 bytes.

[Specification format]

-ALIGNED_SECTION=section[,section]...

 

-

Interpretation when omitted

None

[Detailed description]

-

This option changes the number of alignment of section section to 16 bytes.

[Example of use]

-

To change the number of alignment of section A to 16 bytes, describe as:

>rlink a.obj b.obj -aligned_section=A

[Remark]

-

If the -form={object|relocate|library} option and the -extract or -strip option is specified, this option will be invalid.