-NOLOgo


This option suppresses the output of the copyright notice.

[Specification format]

-NOLOgo

 

-

Interpretation when omitted

The copyright notice is output (It is the same result as when the -logo option is specified).

[Detailed description]

-

This option suppresses the output of the copyright notice.

[Example of use]

-

To suppress the output of the copyright notice, describe as:

>rlink a.obj b.obj -nologo