-EXIt


This option specifies the end of option specifications.

[Specification format]

-EXIt

 

-

Interpretation when omitted

None

[Detailed description]

-

This option specifies the end of option specifications.

[Caution]

-

This option can be used only in a subcommand file.

[Example of use]

-

Create subcommand file "test.sub" with the following content.

input=a.obj,b.obj               ;(1)
start=P,C,D/100,B/8000          ;(2)
output=a.abs                    ;(3)
exit

 

To specify subcommand file test.sub, describe as:

>rlink -subcommand=test.sub -nodebug

 

Processing from (1) to (3) are executed and a.abs is output.

The -nodebug option specified on the command line after this option is executed is invalid.