The location counter value, code, line number, and source program under assembly is output.
The output example of the assemble list is shown below.
(1) (2) (3) (4)
OFFSET CODE NO SOURCE STATEMENT
00000000 1 #CC-RH Compiler RH850 Assembler Source
00000000 2 #@ CC-RH Version : VX.XX.XXx [DD Mmm YYY]
00000000 3 #@ Command : main.c -Xcommon=rh850 -S
00000000 4 #@ compiled at Sun Jan 1 00:00:00 2012
00000000 5 .cseg text
00000000 6 ld.w $_data,r12
00000000 440E0000 -- movhi 0x0,gp,r1
00000004 21670100 -- ld.w 0x0[r1],r12
00000008 7
00000000 8 .dseg data
00000000 00000000 9 _data: .dw 0
00000004 10
|
|
|
|
|
|
Location counter value
The location counter value for the beginning of the code generated for the source program of the corresponding line is output.
|
|
|
Code
The code (machine language instruction or data) generated for the source program of the corresponding line is output.
Each byte is expressed as 2-digit hexadecimal number.
|
|
|
Line number
The number of the line is output.
This is expressed in a decimal number.
|
|
|
Source program
The source program of the line is output.
If instruction expansion is performed for the instruction at that line, the disassembly of the array of machine language instructions generated after the instruction expansion is displayed after "--".
Compiler information (lines 1 to 4) is output only when an assembly source file output from the compiler is assembled.
|